Technical FAQs

Ask a Question

"The PatchInstaller failed to complete successfully. Please re-run the install. Setup will now end." error message appears during a System Manager Software (SMS) 4.3 upgrade

Goals and Symptoms

Symptoms
The following error message appears during step 2 of the System Manager Software (SMS) 4.3 upgrade:

The PatchInstaller failed to complete successfully. Please re-run the install. Setup will now end.




The user is also running eSolutions software PRODUCTS such as Active Pager Module (APM) or Sequence of Events Recorder (SER).

Causes and Fixes

Cause

eSolutions services for either Active Pager Module, Sequence of Events Recorder, or both are running.


Resolution

Stop all eSolutions services via the eSolutions Service Controller and re-run the SMS install.




Note: The eSolutions Service Controller can be access by double-clicking on the red dragon icon in the Windows task bar.


Legacy KB System (APS) Data: RESL200068 V1.0, Originally authored by MaTh on 09/23/2009, Last Edited by MaTh on 09/23/2009
Related ranges: System Manager 4.3
Was this helpful?
What can we do to improve the information ?