Technical FAQs

Ask a Question

What are the Overcurrent Ratings (Overcurrent Withstand) for the E4800?

The Overcurrent Withstand for the E4800 are:
10 A continuous
50 A @ 10 seconds/hour
120 A @ 1 second/hour


Legacy KB System (APS) Data: RESL199888 V1.0, Originally authored by MaTh on 09/09/2009, Last Edited by MaTh on 09/09/2009
Related ranges: E4800
Was this helpful?
What can we do to improve the information ?