Technical FAQs

Ask a Question

Can SMSOPC (Matrikon OPC) be run as a service?

Note: In version of Matrikon OPC for System Manager Software, the default install option is to run the program as a service.
Yes, to run SMSOPC as a service, follow these steps:

1. In a windows command prompt, browse to C:\Program Files\Matrikon\OPC\System Manager (TM)\
2. Type: "opcsms.exe -unregister"and press enter
3. Type: "opcsms.exe -regserver" and press enter
4. Type: "opcsms.exe -service" and press enter
5. Go to Control Panel > Administrative Tools > Services
6. Right-click on "Matrikon OPC Server for System Manager (TM)" and choose properties
7. Set the service to start automatically and start the service

Was this helpful?
What can we do to improve the information ?