Technical FAQs

Ask a Question

What are the part numbers for Branch Current Monitor (BCM) ribbon cables?

Part numbers for the Branch Current Monitor (BCM) ribbon cables:
CBL008 -> 18" length
CBL016 -> 48" length
CBL017 -> 60" length
CBL018 -> 72" length
CBL019 -> 97" length
CBL020 -> 120" length
CBL021 -> 240" length

Please note that these are numbers are for a single cable. If both ribbon cables are needed, these part numbers must be orders in pairs.


Legacy KB System (APS) Data: RESL199735 V1.0, Originally authored by MaTh on 08/28/2009, Last Edited by MaTh on 08/28/2009
Related ranges: BCM (Branch Current Monitor)
Was this helpful?
What can we do to improve the information ?