Technical FAQs

Ask a Question

Getting Started With ION Enterprise GPRS Modem Connections

Goals and Symptoms

Basic instructions to configure ION Enterprise to connect to a meter through a wireless (GPRS) modem.

Causes and Fixes

Example settings for the MultiTech GPRS MultiModem are given. Please see attached Application Note document from the Global PMC Application Expertise Team (Schneider Electric Industries SAS - Power Business Unit).

Attachments

(Removed File URL: 199713_C85A/Getting_Started_With_ION_Enterprise_GPRS_Modem_Connections_V1.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/7553f3c5e326ff2ec125761e0010cbed/fl_block_5/0.544?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL199713 V1.0, Originally authored by KBAdPM on 08/26/2009, Last Edited by KBAdPM on 08/26/2009
Related ranges: ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?