Technical FAQs

Ask a Question

When configuring the delay for onboard alarms in a Power Meter or Circuit Monitor, what are the units associated with the pickup and dropout values?

Issue
A user when configuring the delay for onboard alarms in a Power Meter or Circuit Monitor, would like to know the units associated with the pickup and dropout values.

Product Line
Power Meters
Circuit Monitors

Environment
Circuit monitor/ power monitor settings

Cause
Associated units and values

Resolution
For standard speed alarms, the delay is defined in seconds.
For high speed alarms, the delay is defined in increments of 100ms.
For disturbance alarms, the delay is defined in cycles. 

For example, a delay of 5 for standard alarms equates to 5 second. For high speed alarms, a delay of 5 equates to 500ms. For disturbance alarms, a delay of 5 equates to 5 cycles.

Was this helpful?
What can we do to improve the information ?