Technical FAQs

Ask a Question

I can’t find the Project DBF Add-In tool of PowerLogic SCADA in my MS Excel 2003.

First, you need to check whether the tool has been installed well or not.

     1. Find the tool from Add or Remove Programs of Control Panel as below.

       

         If you cant, you need to install that component from your PowerLogic SCADA CD.

 

     2. If you can find the tool there, you need to go to MS Excel to check other property.

         Go to Help à About Microsoft Office Excel

     

         And then Click Disabled Items below.

      

 If you can find the DBF Add-In item at the Disabled Items window below, you need to enable it.

 

---

Last Revised: 22-July-2009

Applies To: PowerLogic SCADA 7.1

Original Author: YJ

Published By: DRM

Public

All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL199485 V2.0, Originally authored by KBAdPM on 07/28/2009, Last Edited by DaMi on 07/31/2009
Related ranges: PowerLogic SCADA 7.1
Was this helpful?
What can we do to improve the information ?