Technical FAQs

Ask a Question

ION EEM Virtual Source will not totalize if the timestamp is not the exact same for different sources.

If one device has a timestamp of 8:00:00am and the other device assigned to the virtual source has a timestamp of 8:00:01am the virtual meter will not totalize at 8:00:00am because the virtual meter sees the second timestamp as a gap in the data. Make sure that jitter correction is turned on for the sources to make sure that all the timestamps will be on the hour readings in the virtual source. Jitter Correction can be turned on in the ION EEM Admin Tool under the Data Import page.

Date Created: July 22, 2009
Last Revised: July 22, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL199433 V1.0, Originally authored by MiNe on 07/23/2009, Last Edited by MiNe on 07/23/2009
Related ranges: EEM V3.9, EEM V3.95
Was this helpful?
What can we do to improve the information ?