Technical FAQs

Ask a Question

How to access Sybase Data with ION Enterprise that is in multiple Sybase databases.

Goals and Symptoms

Please follow the technical note titled "Accessing Sybase Data with ION Enterprise" in order to make the initial connection to the first database. In order to connect to an additional database follow the procedure found below.

Facts and Changes

Keywords:
more than one
more than 1
2 databases
Sybase
Service Configuration Parameters
SQL Anywhere
ION Enterprise
Archive
Query

Causes and Fixes

1) Open Sybase Central (Start > Programs > SQL Anywhere > Sybase Central)
2) Right click on the service that was created while following the technical note and choose properties and click on the configuration tab.
3) Copy the path and file name from the configuration and paste them below
ex. The code in the file is something like:
n PCNAME_DB_SERVER
c 12M
x netbios,tcpip
C:\Program Files\Sybase Database\PML_LOGS.DB
-n PML_LOGS

copy the last 2 lines here and paste below:

n PCNAME_DB_SERVER
c 12M
x netbios,tcpip
C:\Program Files\Sybase Database\PML_LOGS.DB
-n PML_LOGS
C:\Program Files\Sybase Database\PML_LOGS.DB
-n PML_LOGS

4) Now edit the path to the other database that needs to be connected and give it a unique name:
n PCNAME_DB_SERVER
c 12M
x netbios,tcpip
C:\Program Files\Sybase Database\PML_LOGS.DB
-n PML_LOGS
C:\Program Files\Sybase Database\PML_Archive.DB
-n PML_Archive

5) Now click apply and restart the SQL Anywhere Service.
6) Now create a new database connection with the parameters shown below [Control Panel > Administrative Tools > Data Sources (ODBC)]

Note: the Data Source Name can be changed to be anything

7) Now create a new query module in ION Enterprise Designer as described in the technical note and connect to the Data Source Name created in step 6:



Now the data can be viewed for both databases in ION Enterprise Vista. Repeat the procedure to add more databases to the system.

Attachments

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/5d57ae6d82d8ae5bc12575cc00109b8c/fl_block_5/0.1A60?OpenElement&FieldElemFormat=gif)
Date Created: June 4, 2009
Last Revised: June 4, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL199086 V1.0, Originally authored by MiNe on 06/05/2009, Last Edited by MiNe on 06/05/2009
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0
Was this helpful?
What can we do to improve the information ?