Technical FAQs

Ask a Question

Will ION Enterprise v5.6 work with touch screen computers?

It is possible to run ION Enterprise v5.6 on computers with touchscreens. A touchscreen is just like a mouse, so for basic operations in Vista or WebReach it will work just fine. Touchscreen systems also have built-in "soft keyboards" that pop up onscreen and they can type almost like a regular keyboard.
For more involved operations like using Designer or creating custom diagrams (which require fine cursor control), it would be much easier to plug a keyboard and mouse into the computer and use those.

Date Created: October 28, 2008
Last Revised: May 6, 2009
Public
Original Author: MN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL198448 V1.0, Originally authored by MiNe on 05/06/2009, Last Edited by MiNe on 05/06/2009
Related ranges: ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?