Technical FAQs

Ask a Question

In Windows XP, the User Needs to Set Permissions on a File or Folder, but There Is No Security Tab in Properties

This issue occurs in Windows XP. By default, the Security tab is hidden.

To enable the Security tab, the user must disable simple file sharing by following these steps:      

1) In Windows Explorer, go to Tools and choose Folder Options….

2) Click the View tab.

3) At the bottom of Advanced Settings, uncheck Use simple file sharing (Recommended).

4) Click Apply and then OK.

The user now has access to the Security tab.


Legacy KB System (APS) Data: RESL198195 V1.0, Originally authored by AnVa on 04/01/2009, Last Edited by AnVa on 04/01/2009
Related ranges: OS & related Third Party PRODUCTS for Power Mangement Systems
Was this helpful?
What can we do to improve the information ?