Technical FAQs

Ask a Question

How to Simulate Events in SER Using a CM4000 or Monaghan ProTime Sequence of Events Module


CM4000 (CM4)

To simulate descrete input switching(On and Off), use SMS, PAE generic Modbus/Jbus Tester or some other Modbus utility write holding registers:

 

Modbus Register Value

8000 32333 command to begin input simulation mode.

8001 9999

8002 1 or 2 for number of seconds on

8003 1 or 2 for number of seconds off

 

 

 

Protime

Test mode is entered by writing to the holding register 1577 as indicated below:

 

Modbus Register Value

1577 21930 test mode on

 

To disable test mode.

1577 set to any other value to turn off test mode.

        • OR ten minutes will turn off.

Writing a value of 21930 decimal to register number 1577 will cause the ProTime module to simulate status input changes for a period of approximately 15 minutes. This can be useful for testing to see that events from an SER module are being recorded by the SER software.

Keywords: Sequence of Events Recording, Sequence of Events Recorder, SER 6.0, 6.3, 7.0, 7.1

Legacy KB System (APS) Data: RESL198177 V2.0, Originally authored by AnVa on 04/01/2009, Last Edited by MaTh on 09/28/2011
Related ranges: Sequence of Events Recorder (SER)
Was this helpful?
What can we do to improve the information ?