Technical FAQs

Ask a Question

Can Paging on Communications Loss Be Disabled in Active Pager Module (APM) Version 6.0?

Paging on Communications Loss can be disabled in APM 6. To do so, edit the filter in the setup menu.
The procedure is as follows:

  1. Go to Setup > APM Setup from the top menu.
  2. Under Setup on the left side of the window, select Filter and then click Edit.
  3. In the Available Nodes box, click on the plus sign of the desired meter.
  4. Uncheck the Comms Loss box.
  5. Repeat steps 2 and 3 for all meters if no communications loss notification is desired.
  6. Click the Save Filter button.
  7. Click on System located on the left side of the screen, then Preferences.
  8. Restart the SMS OPC Server and APM Service by clicking the Restart Services button.


Legacy KB System (APS) Data: RESL197961 V1.0, Originally authored by AnVa on 03/05/2009, Last Edited by AnVa on 03/05/2009
Related ranges: Paging Module
Was this helpful?
What can we do to improve the information ?