Technical FAQs

Ask a Question

Advanced Reports (AR) does not support CSV format for reports with cross-tabs. It causes an error: Crystal Reports: Print Engine Error


Cause:
Advanced Reports uses Crystal Enterprise 10 and it does not support exporting reports to CSV (Character-Separated Values) format when the report has cross-tabs (table) controls. Tables like the 100msec report, all Usage Reports, and Table Reports use cross-tabs. Because of this, scheduling a report and selecting the format of the report to Character-separated Values (csv) will cause the following error "Crystal Reports: Print Engine Error".

Solution:
Select Microsoft Excel as the format then convert the Excel file to a CSV in Excel.

Note: CSV file format refers to "Character-Separated Values" in Crystal Reports and "Comma Separated Values" (or Variables) in Microsoft Excel.




Date Created: October 21, 2008
Last Revised: October 21, 2008
Public
Original Author: PH/KT
All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL193007 V1.0, Originally authored by PhHa on 10/26/2008, Last Edited by PhHa on 10/26/2008
Related ranges: SMS Add-on, System Manager 4.0, System Manager 4.2
Was this helpful?
What can we do to improve the information ?