Technical FAQs

Ask a Question

Is ION Enterprise 5.6 supported on Windows Vista?

For an ION Enterprise 5.6 server installation, the only supported operating systems are Windows XP or 2003, as stated in the Commissioning Guide. Our ION software has not yet been formally tested with Windows Vista, thus full support can not be provided for Windows Vista installations.

Last Revised: March 4, 2008
Applies To: ION Enterprise 5.6
Original Author: KG
Public
All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL191337 V1.0, Originally authored by KBAdPM on 03/04/2008, Last Edited by KBAdPM on 03/04/2008
Related ranges: ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?