Technical FAQs

Ask a Question

Can ION Enterprise be installed without xp_cmdshell?

xp_cmdshell is used to send a "netsend" message. Netsend is used in the Database Manager to send Alerts when database maintanace has failed/completed. It's presence is not mandatory for the installation of ION Enterprise.

Last Revised: February 18, 2008
Applies To: ION Enterprise
Public
All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL191117 V1.0, Originally authored by KBAdPM on 02/19/2008, Last Edited by KBAdPM on 02/19/2008
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5
Was this helpful?
What can we do to improve the information ?