Technical FAQs

Ask a Question

Can Advanced Reports (AR) be installed after System Manager Software (SMS) Service Update 3 (SU3)?

Advanced Reports can be installed after SU3 has been applied to SMS v 4.0 . However, SU3 must be re-installed after completion of the AR installation.


Legacy KB System (APS) Data: RESL191107 V1.0, Originally authored by PhHa on 02/15/2008, Last Edited by PhHa on 02/15/2008
Related ranges: System Manager 4.0, SMS Add-on
Was this helpful?
What can we do to improve the information ?