Technical FAQs

Ask a Question

IP31 sealing kit reference 08711: Why use the slotted plate only at bottom of the cubicle? Nothing forecasted for the top?

We hide only the bottom holes to avoid the bounce of the dropelets on the ground to enter through the bottom holes, but impossible through the top holes.


Legacy KB System (APS) Data: RESL190417 V2.0, Originally authored by SeOs on 12/19/2007, Last Edited by GwPo on 06/16/2010
Related ranges: Prisma Plus
Was this helpful?
What can we do to improve the information ?