Technical FAQs

Ask a Question

What is the Maximum Surge Withstand on the Analog I/O For a 76xx/75xx?

The Analog Inputs and Outputs are isolated to 750V. There is no grounding inside the meter for the analog I/O's. These circuits are isolated from the internals (CPU, etc) of the meter.
Refer to the datasheet http://www.pwrm.com/PRODUCTS/ION7650.




Last Revised: December 3, 2007
Applies To: ION 7500 / 7600, 7550 / 7650
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL190147 V1.0, Originally authored by KBAdPM on 12/04/2007, Last Edited by KBAdPM on 12/04/2007
Related ranges: ION7550/ION7650, ION7500/ION7600
Was this helpful?
What can we do to improve the information ?