Technical FAQs

Ask a Question

Is ION Enterprise 5.6 supported on a Windows 2003 Small Business Premium Edition OS?

Yes, it is supported. The "Windows 2003 Small Business Premium edition" comes with SQL 2005 Standard Edition bundled into it.

Last Revised: November 28, 2007
Applies To: ION Enterprise
Controlled
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189817 V1.0, Originally authored by KBAdPM on 11/28/2007, Last Edited by KBAdPM on 11/28/2007
Related ranges: ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?