Technical FAQs

Ask a Question

Is ION Enterprise 5.6 supported on Windows 2000 Server?

No, Windows Server 2000 is not supported with ION Enterprise 5.6.
One problem that we have seen is that the real-time data in Webreach does not show up, but the historical data works. In this case, the resolution is to upgrade to the MDAC version (2.8 SP1).

However, there are likely other problems with running ION Enterprise 5.6 on Windows Server 2000 that have not yet been encountered.

If you are upgrading ION Enterprise from an earlier version or installing a new copy ION Enterprise 5.6, either upgrade Windows 2000 or install it on one of the Operating Systems we suggest.
i.e. Windows 2003 Server or Windows XP




Last Revised: December 12, 2007
Applies To: ION Enterprise
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189711 V2.0, Originally authored by KBAdPM on 11/26/2007, Last Edited by DeCr on 12/13/2007
Related ranges: ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?