Technical FAQs

Ask a Question

What is the sequence of upgrading ION Enterprise 5.5 and SQL 2000 to ION Enterprise 5.6 and SQL 2005?

The sequence to follow should be:

  1. Upgrade ION Enterprise 5.5 to 5.6 first, leaving SQL 2000 intact.
  2. Check that the system is working properly and as expected. Check historic logging, in particular.
  3. After checking the Enterprise system, upgrade SQL 2000 to SQL 2005.

Each step might have different scenarios, therefore please refer to relevant upgrade path which fits to the existing system.




Last Revised: November 22, 2007
Applies To: ION Enterprise
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL189510 V1.0, Originally authored by KBAdPM on 11/23/2007, Last Edited by KBAdPM on 11/23/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5
Was this helpful?
What can we do to improve the information ?