Technical FAQs

Ask a Question

How to connect ION Setup to a meter using a Utiliprob Optical coupler.

Connect the Utiliprobe to the serial port on the back of your computer and the power supply connection to the PS/2 port on the computer.

  1. Start the computer, and open ION Setup.
  2. Use single device configuration mode, and make a serial device connection.
  3. Check the Serial port settings under the Timings tab:
    RTS/CTS = Toggle
    DTR = Disabled
  4. Establish a connection. ION Setup should automaticly determine Baud/Unit ID.

NOTE: If you are having difficulties with connecting, confirm that the device protocol is set to ION




Last Revised: November 19, 2007
Applies To: ION Setup
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL189303 V1.0, Originally authored by KBAdPM on 11/20/2007, Last Edited by KBAdPM on 11/20/2007
Related ranges: ION Setup 2.1
Was this helpful?
What can we do to improve the information ?