Technical FAQs

Ask a Question

How do I reset my meter to a factory default framework using ION Enterprise?

Open the meter in Designer (opened from Management Console) and follow this procedure:

  1. Select the Edit menu and choose 'Select All'.
  2. Press the delete button.

    NOTE: A popup will appear warning you that 'CORE' modules cannot be deleted, this is normal.
  3. Select the Edit menu and choose 'Paste from Framework'.
  4. Choose the meter framework file that you would like to paste to the meter (located in the ...\ION Enterprise\config\fmwk\nd folder).
  5. Goto File menu and select Send & Save to the meter.
  6. Goto the Program files directory and follow the direcory structure to the following location:

    ...Program Files\Schneider Electric\ION Enterprise\config\diagrams\nd
  7. Delete the device from the files in the folder.

    NOTE: The file will be re-created when you connect to the device in designer next time.




Last Revised: November 19, 2007
Applies To: ION Enterprise
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL189298 V1.0, Originally authored by KBAdPM on 11/20/2007, Last Edited by KBAdPM on 11/20/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0
Was this helpful?
What can we do to improve the information ?