Technical FAQs

Ask a Question

How to adjust the Vista Update rate

To adjust the meter's Vista update rate for ION Enterprise 5.5 and below you can follow this procedure:

  1. Open Managment Console
  2. Go to the Meter Site
  3. Right click on device > Properties
  4. Right click on the dark grey area and choose 'Advanced Properties'
  5. Goto the 'Update Rate' and change it from 1/2 second (500ms) to your desired value.

NOTE: This is a minimum update rate, the refresh from the meter may take longer depending on circumstances (i.e.: Comm server backlog, networking delays etc.)




Last Revised: November 16, 2007
Applies To: ION Enterprise
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL189284 V1.0, Originally authored by KBAdPM on 11/17/2007, Last Edited by KBAdPM on 11/17/2007
Related ranges: ION Enterprise V5.5, ION Enterprise V5.0, ION Enterprise V4.5, ION Enterprise V4.0
Was this helpful?
What can we do to improve the information ?