Technical FAQs

Ask a Question

Are the GE 3710 and GE 3720 Compatible with ION Enterprise?

The GE 3710 was only shipped with Modbus protocol (Identical to the 3710 ACM meter's Modbus implementation), so by creating a Modbus Device Importer (MDI) file in ION Enterprise you will be able to add the device.
The GE 3720 was selectable between PML & ModbusRTU, so it can be added to ION Enterprise by changing the protocol to PML, or creating an MDI file.



Last Revised: November 13, 2007
Applies To: ION Enterprise, 37xx ACM
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189169 V1.0, Originally authored by KBAdPM on 11/14/2007, Last Edited by KBAdPM on 11/14/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0, 3720 ACM, 3710 ACM
Was this helpful?
What can we do to improve the information ?