Technical FAQs

Ask a Question

Install Shield error '432' when trying to install ION Setup 2.1

This appears to be an Install Shield error. The following KB article resolvs the issue:
http://consumer.installshield.com/kb.asp?id=Q110613




Last Revised: November 13, 2007
Applies To: ION Setup
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189161 V1.0, Originally authored by KBAdPM on 11/14/2007, Last Edited by KBAdPM on 11/14/2007
Related ranges: ION Setup 2.1
Was this helpful?
What can we do to improve the information ?