Technical FAQs

Ask a Question

Do the 37xx ACM meters support DNP protocol?

The 3710 can support DNP, but will likely require a CMOS firmware chip to be swapped out.
The 3720 does not support DNP.

The 3710 CMOS firmware chip can be ordered through the RMA department or your regional BDS representative.




Last Revised: November 13, 2007
Applies To: ACM 37xx
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189160 V1.0, Originally authored by KBAdPM on 11/14/2007, Last Edited by KBAdPM on 11/14/2007
Related ranges: 3720 ACM, 3710 ACM
Was this helpful?
What can we do to improve the information ?