Technical FAQs

Ask a Question

ION 7700 DSP and CPU LEDs are on constantly.

This indicates that the meter's motherboard has frozen. Try to powercycle the meter, but if the problem persists attempt a Firmware upgrade or RMA the device.

Last Revised: November 13, 2007
Applies To: ION 7700
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189156 V1.0, Originally authored by KBAdPM on 11/14/2007, Last Edited by KBAdPM on 11/14/2007
Related ranges: ION7700
Was this helpful?
What can we do to improve the information ?