Technical FAQs

Ask a Question

Does DDE work with Open Office?

Although DDE is supposed to work with Open Office, the multi-platform free-of-charge open source office suite (see their website http://www.openoffice.org/), it has never been tested with ION Enterprise. Importing/Exporting data between ION Enterprise and Open Office should work, but is not supported.

Last Revised: November 13, 2007
Applies To: ION Enterprise
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189147 V1.0, Originally authored by KBAdPM on 11/13/2007, Last Edited by KBAdPM on 11/13/2007
Related ranges: ION Enterprise V5.5, ION Enterprise V5.0, ION Enterprise V4.5, ION Enterprise V4.0, ION Enterprise V5.6
Was this helpful?
What can we do to improve the information ?