Technical FAQs

Ask a Question

What is the firmware upgrade order for the ION 7700, MGT and Xpress card?

Recommended upgrade order:

  1. Xpress
  2. 7700
  3. MGT

If your communications is working with your current Xpress/7700 combination you should be able to upgrade both sides in either order, but it is recommended that you upgrade the Xpress side first so that all ION modules are restored correctly.

NOTE: some earlier versions of 7700/Xpress do not support upgrading the Xpress through COM1.

Downgrading is not recommended.




Original article#8478
Last Revised: October 30, 2007
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL189033 V1.0, Originally authored by KBAdPM on 11/09/2007, Last Edited by KBAdPM on 11/09/2007
Related ranges: ION7700
Was this helpful?
What can we do to improve the information ?