Technical FAQs

Ask a Question

Will ION Enterprise 5.5 Clients work with an ION Enterprise 5.6 Server?

No, there are too many architecture changes between the two versions (Vista and Designer) for a 5.5 Client to be able to connect to a 5.6 Primary. It's possible that Management Console and Reporter will work, but these are untested and unsupported scenarios.

Last Revised: October 16, 2007
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188586 V1.0, Originally authored by KBAdPM on 10/24/2007, Last Edited by KBAdPM on 10/24/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5
Was this helpful?
What can we do to improve the information ?