Technical FAQs

Ask a Question

Can Webreach work on a Mac?

Troubleshooting any Enterprise component on a Mac is beyond the scope of ION Enterprise support.
Microsoft stopped development on Internet Explorer for Mac's in 2003 so it's possible that the latest version of browser for the Mac may not support the necessary technologies (graphing will definitely not work):

  • ASP
  • XML stylesheet transforms
  • JavaScript
  • XML Data Islands

The above components are critical for the operation of Webreach.

If IE for Mac does not work, it may be possible to run a Windows emulator to get the latest version of Internet Explorer working on the Mac. Another option would be to try another browser such as Safari, Firefox or Opera, but they are also untested and unsupported.




Last Revised: October 15, 2007
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL188584 V1.0, Originally authored by KBAdPM on 10/24/2007, Last Edited by KBAdPM on 10/24/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0
Was this helpful?
What can we do to improve the information ?