Technical FAQs

Ask a Question

Can Data Recorder information be accessed using the DNP 3.0 protocol?

No, the DNP 3.0 protocol is unable to access the information stored in data recorders.

Use the ION protocol to access historic data in the data recorders.




Last Revised: October 15, 2007
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL188487 V1.0, Originally authored by KBAdPM on 10/17/2007, Last Edited by KBAdPM on 10/17/2007
Related ranges: ION8800, ION8600, ION7550/ION7650, ION7300, ION8500, ION8400, ION8300, ION7700, ION7500/ION7600
Was this helpful?
What can we do to improve the information ?