Technical FAQs

Ask a Question

Can the Hotfix for Internet Explorer 7 be installed any time or only after IE7 is installed?

No, the hotfix is not effective if installed prior to IE7 upgrade. It however should not negatively affect the IE7 upgrade, and can be re-run after the upgrade has been complete to allow Webreach to operate correctly.

More Information

http://www.pwrm.com/support/IONEnterprise/downloads/#HotfixInternetExplorer7

 

 

Original article#16727

Last Revised: June 22 2007

Public

All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL186708 V1.0, Originally authored by KBAdPM on 07/06/2007, Last Edited by KBAdPM on 07/06/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0
Was this helpful?
What can we do to improve the information ?