Technical FAQs

Ask a Question

ION Enterprise 5.5 Commisioning Guide Clarification

Goals and Symptoms

On page 29, in the intro to Stage 2 - Install ION Enterprise, it says.
"Also ensure that your user account is not in use on any other

workstations before you start this installation". Can someone explain

why this would matter?

Causes and Fixes

This is probably a leftover from previous versions of ION Enterprise. There should be no problem using this account, as long as it has full Admin privileges on the machine they're installing to.

A review of this section is now underway to determine if it should be removed from the commissioning guide.



 

More Information

As of May 29, 2007 this statement has not been changed. The latest revision of the ION Enterprise 5.5 commisioning guide is dated as November 2006:

 

http://www.pwrm.com/support/IONEnterprise/

Attachments

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/04fe720fae0971bdc125731000162052/fl_block_5/0.1AD6?OpenElement&FieldElemFormat=gif)
Original article#16723

Last Revised: June 22 2007

Public

All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL186639 V1.0, Originally authored by KBAdPM on 07/06/2007, Last Edited by KBAdPM on 07/06/2007
Related ranges: ION Enterprise V5.5
Was this helpful?
What can we do to improve the information ?