Technical FAQs

Ask a Question

What Columns need to be present to allow Meter Event Log operation? (The beep/flash settings aren’t working)

Meter event log needs to have the following columns present to operate correctly:
timestamp

cause_ion

cause_value

effect_ion

effect_value

priority

ack_time

recordID

node.

 

These columns will allow you to setup the meter event log to trigger flashes/beeps/popups similar to Global Event Viewer.

 

 

Original article#16714

Last Revised: May 29 2007

Public

All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL186626 V1.0, Originally authored by KBAdPM on 07/06/2007, Last Edited by KBAdPM on 07/06/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5
Was this helpful?
What can we do to improve the information ?