Technical FAQs

Ask a Question

The first custom quantity created does not update on GFX screens

SMS 3.x only

The first custom quantity created in System Manager Software (SMS) 3.x will not display correctly on a GFX diagram. It will appear as if it is not being updated. After creating the custom quantity, save the changes and then go back in and delete it. Next, create a new custom quantity with the same name and reassign the GFX block to that quantity. This has been corrected in SMS 4.x.

Legacy KB System (APS) Data: RESL186122 V2.0, Originally authored by KBAdPM on 07/04/2007, Last Edited by MaTh on 10/07/2010
Related ranges: System Manager 3.1, System Manager 3.2, System Manager 3.3
Was this helpful?
What can we do to improve the information ?