Technical FAQs

Ask a Question

Active Alarms are not reporting in System Manager Software (SMS) from Series 2000, 3000, 4000 Circuit Monitors or Series 600, 800 Power Meters. The meter's front display indicates that the alarms is active.

 

The most common cause for alarms not coming into System Manager Software (SMS) from a device is when the onboard alarm log records are set to 0 (zero). Go to Setup>Device/Routing>configuration then verify that the number of records for the "alarm log" is not zero, 0. Verify that the alarm log is enabled.

This applies to the Series 2000, 3000, 4000 Circuit Monitors and Series 600, 800 Power Meters.
System Manager Software (SMS) v 3.3.x.x and 4.x




Date Created: Unknown
Last Revised: March 19, 2008
Public
Original Author: PMOZONE/PH
All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL185061 V2.0, Originally authored by KBAdPM on 06/27/2007, Last Edited by PhHa on 03/20/2008
Related ranges: System Manager 3.3, System Manager 4.0, System Manager 3.2
Was this helpful?
What can we do to improve the information ?