Technical FAQs

Ask a Question

Designer Error When Adding Module

Goals and Symptoms

Summary
When adding a module in ION Designer the operator receives the following error:

 

'You do not have authority to make configuration changes to this node diagram'

 

Symptoms

An error pops up when adding a module in designer (See above).

Facts and Changes

Keywords
Designer, Error, Permissions

Causes and Fixes

Cause
Users Windows logon has incorrect permissions (Possibly Power User and not Administrator).



 

Resolution

Check User preferences

 

For Windows 2003 Server:

Admin tools -> Security Options -> User Accts

 

For Windows XP:

 

Start -> Control Panel -> User Accounts

 

Make sure that the user is in the Administrators Group and not another selection (IE: 'Power User').

Attachments

Original article#16716
Last Revised: May 29 2007

Public

All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL184923 V1.0, Originally authored by KBAdPM on 06/22/2007, Last Edited by KBAdPM on 06/22/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0
Was this helpful?
What can we do to improve the information ?