Technical FAQs

Ask a Question

How to set up multilevel alarms in the CM2000 Using SMS

Issue:
End User would like to set up multilevel alarms onboard a CM2000 series power meter using System Manager Software.

Product Line:
CM2000 Series Meter.

Environment:
Onboard Alarming.

Cause: 
Configuring alarms from the front panel may not be apparent to the user. So SMS would seem favorable and can be done remotely. 

Resolution:

See the attached document.

How to setup multilevel alarms in the Series 2000 Circuit Monitor with System Manager Software.pdf

 

Was this helpful?
What can we do to improve the information ?