Technical FAQs

Ask a Question

Selecting an active modem in the SMS database (SQL)

Product Line:
System Manager Software (SMS)

Environment:
SMS Database

Cause:
There are several modems in the System Manager database. The default active modem is the Generic Hayes Compatible. Generic Hayes Compatible should not always be selected.

Resolution:
The attached document contains an example of how to select a different modem as the active modem, if the modem is in the database. 

Was this helpful?
What can we do to improve the information ?