Technical FAQs

Ask a Question

How to start the SQL Agent in the Power Server

To start the SQL Agent service in a Power Server, go to Windows Explorer and double-click on C:\Vega\services.bat. Select the SQLAgent$SMS3000 and click the "Start" button. To ensure that is is set to start automatically, click the "Startup" button and select "Automatic".


© Schneider Electric 2005

Original article#4379
Public


Legacy KB System (APS) Data: RESL184070 V1.0, Originally authored by DaMi on 05/17/2007, Last Edited by DaMi on 05/17/2007
Related ranges: PowerServer
Was this helpful?
What can we do to improve the information ?