Technical FAQs

Ask a Question

Executing AND logic operations using an IOM.

See the attached POWERLOGIC/POWERLINK TECH SUPPORT Application Tip document.
How to Execute AND Logic Operations using an Input Output Module on the Series 2000 Circuit Monitor, Application Tip HW_01_22, May 4, 1999.pdf

Original article#4059
Public


Legacy KB System (APS) Data: RESL184055 V1.0, Originally authored by DaMi on 05/16/2007, Last Edited by DaMi on 05/16/2007
Related ranges: CM2000 series
Was this helpful?
What can we do to improve the information ?