Technical FAQs

Ask a Question

"The control you selected is not registered in your system." appears when trying to add a Multi Input Conditional Graphic block into a GFX screen.

Goals and Symptoms

This message will appear when one the MultiGraphic.ocx file has not been registerd.

Causes and Fixes

Solution:
Register the MultiGraphic.ocx located in c:\program files\common files\Square D shared. To register the file, at a command prompt, change the directory to the above, type in "Regsvr32 MultiGraphic.ocx" without the quotes and press enter.


Version: SMS-XXXX v.3.3.x.x

© Schneider Electric 2005
Original article#4385
Public


Legacy KB System (APS) Data: RESL184054 V1.0, Originally authored by DaMi on 05/16/2007, Last Edited by DaMi on 05/16/2007
Related ranges: System Manager 3.3
Was this helpful?
What can we do to improve the information ?