Technical FAQs

Ask a Question

Can the Powerlogic Meter Configuration Utility (PMCU) be used to configure a Series 2000 Circuit Monitor?

Yes. It is an Optional Install. Run the InstallCM2000.bat located in C:\Powerlogic\PMCU\Optional Install\

Version: PMCU v1.0

© Schneider Electric 2005
Original article#4648
Public


Legacy KB System (APS) Data: RESL183939 V1.0, Originally authored by DaMi on 05/04/2007, Last Edited by DaMi on 05/04/2007
Related ranges: PMCU
Was this helpful?
What can we do to improve the information ?