Technical FAQs

Ask a Question

How to print a waveform capture (WFC) from the System Manager Software (SMS) Web Client version 4.0 and above, or a Power Server Web Client.

 

If you are viewing the waveform capture from the "Alarm" menu, note the time stamp and event for the WFC of interest. Then, select the "Historical" menu and click on the "Waveforms" button. Select the WFC of interest from the list on the left pane of the active window. Opening the WFC from this menu will allow you to interact with the WFC, including printing, copying and saving options.

Original article#4513


Legacy KB System (APS) Data: RESL182927 V1.0, Originally authored by DaMi on 03/20/2007, Last Edited by DaMi on 03/20/2007
Related ranges: SMS 4.x
Was this helpful?
What can we do to improve the information ?