Technical FAQs

Ask a Question

What should be done if the File/Backup feature of the Billing Module v.3.73.xx fails on XP and Windows 2000 machines?

The fix for this issue is to copy the attached zipup23.dll file into the the system32 directory. Depending on the operating system, this directory is either under \WinNT or \Windows. The drive depends on which drive is being used as the boot partition for the operating system.
Example: for Windows 2000 and assuming a standard installation, place the file in c:_winnt_system32


Version: Billing Module v3.73

Reviewed: review complete

Original article#2772
© Schneider Electric 2005


Legacy KB System (APS) Data: RESL182800 V1.0, Originally authored by DaMi on 03/15/2007, Last Edited by DaMi on 03/15/2007
Related ranges: SMS 4.x
Was this helpful?
What can we do to improve the information ?