Technical FAQs

Ask a Question

Billing Module version 3-73 is displaying error 3151 followed by a run time error 13. The column headers are missing as well.

See attached document.
Billing Module version 3-73 is displaying error 3151 followed by a run time error 13-  The column headers are missing as well-.pdf

Original article#2774


Legacy KB System (APS) Data: RESL182794 V1.0, Originally authored by DaMi on 03/15/2007, Last Edited by DaMi on 03/15/2007
Related ranges: SMS 4.x
Was this helpful?
What can we do to improve the information ?