Technical FAQs

Ask a Question

VISTA Error: Too Many Pages

Goals and Symptoms

In VISTA the error message appears saying ''Too Many Pages''.    

Causes and Fixes

Either too many windows are open in VISTA or some diagram has too many grouping objects.

Case 1:
Close all windows.
Go to the Options menu and check 'Browse closes active window'.    
Begin with the network diagram and continue.

Case 2:
Redesign the diagram using fewer grouping objects

 

Original article#9361, SWKB-0509


Legacy KB System (APS) Data: RESL182732 V1.0, Originally authored by DaMi on 03/14/2007, Last Edited by DaMi on 03/14/2007
Related ranges: ION Enterprise
Was this helpful?
What can we do to improve the information ?